AXIS#.SAFEPARAM.SDIn.SAFEINPUT

Description

Indicates which safe input can activate the Safe Direction negative (SDIn) safety function. When activated, the safety system forbids the axis to move in the negative direction.

Value

Description

0

Not used

1

Safe Input 1 (SIN1)

2

Safe Input 2 (SIN2)

3

Safe Input 3 (SIN3)

4

Safe Input 4 (SIN4)

5

Safe Dual Input 1 (SIN1/SIN2)

6

Safe Dual Input 2 (SIN3/SIN4)

 

Context

For complete SDI information refer to SDI (Safe Direction)

Related safety parameters:

Versions

Action

Version

Notes

Implemented

2-00-00-000

Implemented in SMM revision v0.56

General Information

Type

Read/Write

Units

N/A

Range

0 - 6

Default Value

0 (Not used)

Data Type

Integer

Stored in Non-Volatile Memory

No

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.SAFEPARAM.SDIN.SAFEINPUT

3164h

03h

Unsigned8

-

-

Read/Write

No

AXIS2.SAFEPARAM.SDIN.SAFEINPUT

3264h

03h

Unsigned8

-

-

Read/Write

No